What Is GNSS Compassing?

GNSS compassing uses two GNSS antennas mounted at a known separation (baseline) to determine true heading from carrier-phase measurements. By comparing the phase of satellite signals received at each antenna, the system resolves heading with high accuracy and no dependence on the Earth’s magnetic field. This makes GNSS compassing immune to the magnetic distortions that degrade magnetometer-based heading—a persistent challenge on steel-hulled vessels, armored vehicles, and platforms with significant electromagnetic interference.

Unlike magnetometer-based heading, which requires careful calibration to the host platform’s magnetic environment, GNSS compassing delivers true North-referenced heading at any location on Earth without site-specific setup. It also provides reliable heading when the vehicle is stationary or moving slowly, where inertial-only heading estimation accumulates drift.

COMPARE SPECIFICATIONS

 

THE VECTORNAV ADVANTAGE

ACCURATE HEADING ACROSS COMPACT OR EXTENDED BASELINES

VectorNav's dual-antenna carrier-phase processing delivers precise heading across a range of baseline lengths — 0.30°–0.60° RMS at >0.5 m, 0.15°–0.30° RMS at 1.0 m, and 0.08°–0.15° RMS at 2.0 m. With VectorNav, achieve dependable heading performance even in compact, space-limited mechanical layouts. This flexibility supports integration on platforms from compact UAVs to large marine vessels.

TRUE HEADING AT 400Hz

VectorNav’s dual-antenna GNSS compassing delivers precise, drift-free heading at high update rates of 400 Hz, ensuring stable directional awareness under static and low dynamic conditions. Continuous carrier-phase GNSS corrections maintain heading integrity where inertial-only approaches degrade — preserving accuracy for navigation, control, and pointing applications.

GNSS Compass FAQs

GNSS compassing determines true heading by comparing carrier phase measurements between two GNSS antennas, with no dependence on the Earth's magnetic field. This eliminates the heading errors caused by magnetic distortions from steel structures, motors, power cables, and electromagnetic interference — distortions that are unavoidable on most operational platforms. GNSS compassing also requires no magnetic calibration to the host vehicle and provides consistent accuracy regardless of geographic location or magnetic environment.

Heading accuracy is a function of antenna baseline length. With VectorNav's dual-antenna products, typical performance is 0.30°–0.60° RMS at 0.5 m baseline, 0.15°–0.30° RMS at 1.0 m baseline, and 0.08°–0.15° RMS at 2.0 m baseline. Longer baselines deliver better accuracy, so antenna placement should maximize separation within the platform's physical constraints.

Yes. This is one of the primary advantages over single antenna GNSS/INS heading, which accumulates drift at rest. GNSS compassing provides reliable heading at zero speed, making it essential for applications like SATCOM on-the-move (which must acquire the satellite before moving), static survey, pre-mission alignment, and any platform that spends time stationary between operations.

When GNSS signals are temporarily lost, VectorNav's loosely coupled INS filter maintains heading continuity using inertial aiding. The system bridges short GNSS disruptions — from multipath, terrain masking, or brief interference — without losing heading reference. The duration and accuracy of this bridging depends on the IMU grade: Tactical sensors maintain heading through longer outages with less drift.

GNSS compassing is available on VectorNav's dual-antenna INS products: the VN-300 (Industrial) and VN-310 (Tactical). Both products integrate GNSS compassing with full inertial navigation, so position, velocity, and attitude are delivered as a unified, time-synchronized solution.

Mount the antennas with the longest practical separation and a clear view of the sky. It’s also important that both antennas “see” that same sky, so minimize any obstructions between the two antennas. The baseline between antennas should be measured and configured in the system. VectorNav's support engineering team provides antenna placement guidance for specific platforms, including recommendations for minimizing multipath and optimizing heading accuracy within the platform's physical constraints.

WORK AT VECTORNAV

We're explorers at heart, continually pushing the limits of possible to support out-of-this-world applications and customers. Do you share the desire to discover and define new limits? Learn more about working at VectorNav.