VectorNav Inertial Navigation Systems Earn MIL-STD and DO-160 Certifications

Oct 10, 2019, 23:00 PM by 11 Oct 2019

VectorNav's Tactical Series line of Inertial Measurement Units (IMUs) and GNSS-Aided Inertial Navigation Systems (GNSS/INS) complete independent testing for MIL-STD-810G, DO-160G, MIL-STD-1275E and MIL-STD-461.

Dallas, TX – October 11, 2019 – VectorNav Technologies, a leading provider of inertial navigation systems, has completed a series of MIL-STD and DO-160 qualification tests for its Tactical Series line of IMU and GNSS/INS products. The testing proves the robustness of the Tactical Series to a range of temperature, shock, vibration and other environments, as well as conformance to numerous electrical interface and EMI standards. Together with the unmatched SWaP-C to performance characteristics of the Tactical Series, the testing demonstrates yet another advantage of the Tactical Series for defense and aerospace applications.

“There is high demand for dependable, tactical-grade navigation solutions that perform in challenging environmental and operating conditions,” stated VectorNav Director of Sales and Marketing, Jakub Maslikowski. “As the smallest, most costeffective INS with this level of performance and robustness, the Tactical Series is the superior choice for systems integrators seeking these solutions.”

Testing for the MIL-STD and DO-160 standards was performed by independent, certified testing companies in Plano, TX and Huntsville, AL.

VectorNav Technologies is exhibiting at the Association of the Unites States Army’s (AUSA) Annual Meeting in Washington, D.C., October 14-16, at booth #4029. For additional information on the completed and ongoing MILSTD and DO-160 testing, or to schedule a meeting time during AUSA, contact VectorNav at: email: sales@vectornav.com; tel: +1-512-772-3615; web: www.vectornav.com.

About VectorNav Technologies:

VectorNav Technologies is the leading innovator and manufacturer of embedded navigation solutions using the latest in MEMS inertial sensor and GPS/GNSS technology. Since its founding in 2008, VectorNav has provided systems integrators in the military, aerospace, marine, and robotics industries around the world with SWaP-C optimized, high-performance navigation systems. VectorNav has unique expertise in applying the digital filtering and sensor calibration techniques that have multiple decades of heritage in aerospace applications to the stateof-the-art in MEMS inertial and GPS/GNSS technology.